Can the CM9700 Matrix Series control American Dynamics or other manufacturers analog PTZ cameras?

Issue

Can the CM9700 Matrix Series control American Dynamics or other manufacturers analog PTZ cameras?

Product Line

Pelco Matrix

Environment

CM9700 Matrix Switcher any version

Cause

Third Party camera control.

Resolution

The CM9700 Matrix series supports Pelco P protocol for PTZ camera control. Review the camera manufacturers specification sheet to determine if Pelco P is supported by the camera. If not

directly supported it may be possible to translate Pelco P to a protocol that is supported by the camera. Contact the camera manufacturer for options.