When using a KBD300A Universal keyboard, does the KBD300USBKIT take the place of the KBDKIT?

Issue

Does the KBD300USBKIT take the place of the KBDKIT?

Product Line

Pelco Matrix

Environment

  • CM6800
  • CM6700

Cause

Not sure what kit to use for the KBD300A.

Resolution

No, The KBD300A Universal keyboard requires the use of the KBDKIT for remote keyboard connections.

*NOTE: KBD300USBKIT is used with DVR integration applications. In that specific situation the KBDKIT is not needed.