Issue
What are the key differences between the CM9765, CM9770, CM9780 Series Matrix Switcher/Controller?
Product Line
Pelco Matrix
Environment
- CM9765 Matrix Switcher any version
- CM9770 Matrix Switcher any version
- CM9780 Matrix Switcher any version
Cause
Product Specification
Resolution
The key differences between the CM9765, CM9770, CM9780 Series Matrix Switcher/Controller are matrix bay density.
Single bay density is as follows, keep in mind there can be multiple bays in systems;
Matrix bay | Cameras | Monitors |
CM9765 | 256 | 16 |
CM9770 | 256 | 32 |
CM9780 | 512 | 32 |