How do the analog video outputs work on the DSSRV using the ENC5416?

Issue

Analog video outputs on the Digital Sentry Network Video Recorder (DSSRV).

Product Line

Pelco Video Management

Environment

  • Digital Sentry NVR (DSSRV)
  • ENC5416

Cause

ENC5416 video output support

Resolution

  1. Video Input Connectors (CH1 to CH16, BNC type): Connects to cameras.
  2. External Video Output Connector (Vout1 to Vout2, BNC type): Connects to devices such as VCRs or monitors with a VIDEO IN connector. Through Digital Sentry software, you can select from the following display options:
    • Vout1 as a 1x1, 2x2, or 3x3 matrix displaying input CH1 to CH8.
    • Vout2 as a 1x1, 2x2, or 3x3 matrix displaying input CH9 to CH16.

NOTE: Upper Vout1 and lower Vout1 (upper Vout2 and lower Vout2) are physically connected and recognized as the same connector.

 ENC5416 output diagram

Related articles:
How do I configure the Digital Sentry analog monitor output using DS ControlPoint?
How do you program a camera tour on ENC5416 output 1?