What are the different Pre and Post-Alarm Recording settings in the Endura WS5000 Advanced Software?

Issue

What are the different Pre and Post-Alarm Recording settings in the Endura WS5000 Advanced Software?

Product Line

Pelco Video Management

Environment

Endura WS5000 Advanced Software

Cause

Information about Pre and Post alarm recording.

Resolution

The following settings can be applied to motion and alarm-based recording:

Pre is the amount of time that will be recorded before an event occurs. This is possible due to the buffering method that Endura uses to capture video.

Record (minutes) is a configurable amount of time recording will continue to after an event has ended.

Record until alarm is turned off will immediately end recording when the event ends.