Default IP address of the TXB-N

Issue

What is the default IP address of the TXB-N?

Product Line

Pelco Cameras

Environment

  • TXB-N-P
  • TXB-N-F

Cause

Default IP address for locating IP camera on non DHCP environment.

Resolution

The default IP address of the TXB-N series is 192.168.0.20.