How to save a screen layout as a favorite in the DX8100 HVR and DX8100 Client Software.

Issue

How to save a screen layout as a favorite in the DX8100.

Product Line

Pelco Video Management

Environment

  • DX8100 Series HVR
  • DX8100 Client Software

Cause

Create multiple camera views to monitor various site locations.

Resolution

  1. Drag the cameras into the view panels in the desired layout.
  2. Select FAVORITES at the top of the screen.
  3. Click Add to Favorites. The Add to Favorites dialog box opens.
  4. Type in the name of the favorite.
  5. Click SAVE. The camera layout is added to the favorites.


Figure 1. Favorite Menu List

To view the new entry, from the DX8100 menu bar, click Favorites. The new entry appears in the Favorites list.