How to populate cameras into the view screen on the DX4100 client.

Issue

How to populate cameras into the view screen on the DX4100 client.

Product Line

Pelco Video Management

Environment

DX4104 Series Digital Video Recorder Client Software application

Cause

Assign cameras to view panes

Resolution

  1. On the toolbar, click a display option.
  2. Click a pane to make it active. A red border highlights the pane. See figure 1.

    Figure 1. DX4104 Client View Pane options

     
  3. In the Site Tree, click and drag individual cameras to a view pane. Repeat the process for up to 16 cameras. See figure 2.
    In the Site Tree, click and drag Cameras to a pane. All cameras in the Site Tree are assigned sequentially to the panes.

    NOTE: If you do not want a camera to be viewed, you must replace the camera with another one from a different remote site. If you have only one remote site, you cannot remove a camera from a pane.



    Figure 2. DX4104 Client Site Tree