Is the DX8000 Client compatible with a DX8100 HVR Server?

Issue

Is the DX8000 Client compatible with a DX8100 HVR Server?

Product Line

Pelco Video Management

Environment

  • DX8000 Client
  • DX8100 HVR

Cause

Product compatibility

Resolution

No, You will have to use one of the following clients. DX8100 client, DX series Client or  DS Control Point. 

Here are links to the clients.