Full function, variable speed joystick keyboard that can be used with the DVR5100 Series Digital Video Recorder

Issue

Is there a full function, variable speed joystick keyboard that can be used with the DVR5100 Series Digital Video Recorder?

Product Line

Pelco Video Management

Environment

DVR5100 Series Recorder

Cause

Use desktop keyboard with control pods for full switching and configuration, plus joystick control of PTZ functions.

Resolution

Yes.  The DVR5100 Series Digital Video Recorders have built-in support for the KBD5000 Keyboard with PTZ Control.