Is the IS50 Series Camclosures compatible for mounting to the SWM-GY wall mount

Issue

Will a SWM-GY Wall Mount fit the IS50 Series Camclosures?

Product Line

Pelco Cameras

Environment

  • IS50 Camclosure 2 Series
  • SWM-GY

Cause

Wall mounting options for Camclosure II.

Resolution

The SWM-GY will support the mounting of the IS50 Camclosure with IS50-P. Because there is a color difference between the SWM-GY and the IS50 Camclosure with IS50-P, it is recommended to use the SWM-SR

SWM-SR is a compact wall mount, light gray finish. Can be used with IS50-P for wall mount installation. Can also be adapted for corner or pole applications.