Pole mounting an EH3512 Series Enclosure

Issue

What are the options for Pole mounting an EH3512 Series Enclosure?

Product Line

Pelco Cameras

Environment

  • EH3500 Series Enclosure

Cause

Pole Mounting options

Resolution

The following mounts can be used with Pelco enclosures having a 2-inch (5.08 cm) mounting hole pattern and are capable of supporting up to 40 lb (18.14 kg).

  • EM1109 Medium duty pedestal mount for horizontal or vertical pipe or pole applications. Manually adjustable swivel head and cable feed through hole.
  • EM2000 Medium duty 90 degree J-mount for vertical pipe or pole applications. Manually adjustable swivel head and cable feed through hole.
  • EM2200 Medium duty “hook” mount for horizontal pipe or pole applications. Manually adjustable

For more information please see EM1109/EM2000/EM2200 Mount Product Specification Sheet