Program a preset in the DX4700/DX4800 Series Hybrid Video Recorder

Issue

How do you program a preset in the DX4700/DX4800 Series Hybrid Video Recorder?

Product Line

Pelco Video Management

Environment

DX4700/DX4800 Series HVR

Cause

Set PTZ (Pan, Tilt, Zoom) position for the positioning system.

Resolution

Programming a Preset:

  1. Click a camera pane, and then click PTZ   .
  2. Click the Move , ZOOM, and FOCUS buttons to position, zoom, and focus the camera.
     
  3. Store the preset to a memory location.
    Click SET. The camera is now in the programming mode.
    Click the numbers on the keypad for the preset memory location.
    Click PRESET. The camera’s position, zoom factor, and focus setting are stored to the memory location.
     
  4. Repeat the previous steps (as necessary) to create additional presets for the same camera.
     
  5. Click SET to exit the programming mode.
     
  6. Verify that you can activate the preset.
    Click the Move buttons.
    If you changed the camera’s zoom or focus, verify that the settings are different than the preset settings, and then click the number then PRESET. The camera performs the programmed preset.