Cannot PTZ any cameras using a CM9700 Matrix and a CM9760-CXTA Coaxitron Translator.

Issue

Added a CM9760-CXTA Coaxitron Translator and cannot PTZ any of the connected Spectra Series analog cameras.

Product Line

Pelco Matrix

Environment

  • Spectra 4 (analog)
  • CM9760-CXTA Coaxitron Translator
  • CM9760 Matrix (any version)
  • CM9760-KBD (any version)

Cause

Dip switches were set incorrectly on the CM9760-CXTA Coaxitron Translator.

Resolution

  1. Turn Dip switch 6 to the on position for 4800 Baud with Even Parity.
  2. Turn Dip switch 8 to the on position for Spectra Dome mode.
  3. All other switches on the CM9760-CXTA should remain off.

For instructions with illustration, see page 10 of the CM9760-CXTA Coaxitron Translator manual.