Adding a new monitor(s) to a CM9700 Matrix Switcher using System Manager version 9.03.032.

Issue

Need to add additional monitors to a CM9700 Matrix Switcher.

Product Line

Pelco Matrix

Environment

  • CM9700-CC1 version 9.03
  • Pelco System Manager version 9.03.032

Cause

System has used all currently programmed monitors; verify the system has the hardware installed to support additional monitors.

Resolution

  1. Open the Add Device wizard, and then click the device type in the Select Device Type drop-down box. If a red exclamation symbol appears next to the Select Model drop-down box, click the drop-down box to select the appropriate device.
  2. Click Next. The Video Input/Output Devices page opens.
  3. Specify the number of devices and the physical number range by completing all the fields.
  4. Click Next. The Device Identification page opens.
  5. Specify the device name(s) and logical number range by completing all the fields.
  6. Click Next, and then click Finish on the Add More Devices page.

For instructions with illustration, see pages 29 and 30 of the CM9700-MGR Software Guide.