What is the maximum distance I can install a KBD4000/4002 Keyboard from a Genex multiplexer without using the KBDKIT?

Issue

Install a KBD4000/4002 Keyboard to a Genex multiplexer.

Product Line

Pelco Matrix

Environment

  • KBD4000 all versions
  • KBD4002 all versions
  • Genex Multiplexer all versions

Cause

New installation or relocating Keyboard/Genex

Resolution

The maximum distance is 25 feet with the factory provided cable, any further and you must use the KBDKIT remote keyboard kit.