How to convert the Spectra IV series to a pendant mount model.

Issue

What do I need to convert the Spectra IV series to a pendant mounting?

Product Line

Pelco Cameras

Environment

  • BB4-PG
  • BB4-PG-E
  • LDHQPB-1
  • LDHQPB-0

Cause

Relocating an in-ceiling camera to a pendant style for wall or ceiling mount option.

Resolution

It requires a pendant style backbox and a lower dome.

  • For indoor backbox the part number is BB4-PG
  • For outdoor backbox, part number is BB4-PG-E.  
  • The lower dome part number for either housing is LDHQPB-1(clear bubble) or LDHQPB-0 (smoked bubble)