How to control a Spectra Series camera from Sensormatic system

Issue

Is there a TXB translator board for Sensormatic?

Product Line

Pelco Cameras

Environment

  • Spectra Analog Series
  • TXB-S422

Cause

Protocol Converter for support of Sensormatic to Pelco protocol for Spectra

Resolution

Pelco offers the TXB-S422 for Sensormatic controllers to control the Spectra Series camera.

Compatible Controllers of Sensormatic Electronics Corporation

  • RC58 (VM1-SensorVision)
  • RC216 (VM96-View Manager)
  • AD2083/02 Series American Dynamics protocol translator
  • NOTE: SensorNet is not supported.
  • NOTE: The Spectra IV will auto-sense theSensormatic protocol without additional protocol translator.