Accessories for the KBD300A keyboard.

Issue

What are the optional accessories for the KBD300A keyboard?

Product Line

Pelco Matrix

Environment

KBD300A

Cause

Remote KBD wiring.

Resolution

Part Number Description
KBDKIT Remote keyboard wiring kit. Includes two RJ-45 wall blocks and one 120 VAC to 12 VAC transformer.
KBDKIT-X Same as KBDKIT except includes 230 VAC to 12 VAC transformer.
KBD300USBKIT Wiring kit to attach a KBD300A to a USB port on either the DX4500/DX4600 or DS ControlPoint on the DS DVR.