When configuring an NSM5200 for the first time what address should I use in the Failover IP address field?

Issue

When configuring an NSM5200 for the first time what address should I use in the Failover IP address field?

Product Line

Pelco Video Management

Environment

Endura NSM5200- All versions

Cause

Information regarding the failover IP address on the NSM5200 is needed.

Resolution

Use any IP address that is on the same VLAN as the NSMs that is not being used by any other devices and is not part of the DHCP scope.