Where can I adjust the bandwidth throttle on the DX8000/DX8100 Series video recorder?

Issue

Where can I adjust the bandwidth throttle on the DX8000/DX8100 Series video recorder?

Product Line

Pelco Video Management

Environment

DX8000/DX8100 Series

Cause

Increase bandwidth to decrease video delays.

Resolution

  1. Click on setup menu. Setup dialog appears
  2. Click Network button. The Network page is displayed.
  3. Drag the network bandwidth throttle slider to the desired value. Setting the network bandwidth throttle limit the amount of network resources allocated to client connections.
    • Client bandwidth can be adjusted from a minimum of 64 Kbps to a maximum of 10 Mbps in increments of 64 Kbps.

Note: To utiliize the 100 mbps connection: the bandwidth is available via a check box under the bandwidth throttle slider bar in DX8100 version 2.0.00.2727.

 

Related Topics:

How do I upgrade the DX8100 Series video recorders from software version 2.0.00.2717 to 2.0.00.2727