Can I upgrade a CM6800-32X6 Matrix Switcher by adding another bay?

Issue

Would like to expand a CM6800-32X6 Matrix Switcher.

Product Line

Pelco Matrix

Environment

CM6800-32X6 any version

Cause

More camera inputs are needed.

Resolution

No, it is not possible to connect multiple CM6800-32x6 Matrix Switchers together. 

If additional inputs or outputs are required, upgrade to the CM6800E-48x8 Matrix Switcher.  Two CM6800E-48x8 units can be stacked for a total of 96 inputs and 16 outputs.