What is the default Define PIN for the CM9760-KBD Intelligent Keyboard?

Issue

What is the default Define PIN for the CM9760-KBD Intelligent Keyboard?

Product Line

Pelco Matrix

Environment

CM9760-KBD Intelligent Keyboard all versions

Cause

Need to define a pattern, preset or arm an alarm.

Resolution

The CM9760-KBD Intelligent Keyboard default Define PIN is: 1234