Manual Iris control for the Spectra IV Series dome.

Issue

If I manually close the iris on the Spectra IV Series dome when will it return to auto iris mode?

Product Line

Pelco Cameras

Environment

  • Spectra IV
  • Esprit with IOP
  • Spectra Mini

Cause

Lens responds to manual control for closing and opening.

Resolution

When the Spectra camera receives a pan or tilt command, the Spectra Series camera will return to Auto Iris operation.