What are the PTZ protocol options for Endura NET5401T, NET5402T and NET5404T video encoders?

Issue

What are the PTZ protocol options for Endura NET5401T, NET5402T and NET5404T video encoders?

Product Line

Pelco Transmission & Power

Environment

  • NET5401T
  • NET5402T
  • NET5404T

Cause

Product Specification

Resolution

By default the PTZ control mode is set to Disabled. The PTZ protocol options that the encoder supports are Extended Coaxitron and Pelco D (RS-422).

Version 1.9.2 of the NET5400T firmware introduced support for the Pelco P protocol. Download the latest firmware from the Buildings Download Center to enable support.