How to get PTZ control and make the PTZ cameras move faster using the DX8100 on-screen PTZ control?

Issue

How do I make the PTZ cameras move faster using the DX8100 on-screen PTZ control?

Product Line

Pelco Video Management

Environment

DX8100 Series
PTZ cameras

Cause

When controlling PTZ camera with the arrows on the right side of the display, the camera will move a little slower than using the mouse.

Resolution

To operate the on-screen PTZ controls:

  1. Place the mouse pointer in the middle of the camera's view pane. The mouse pointer will change to a black cross when the on-screen PTZ control is available.
  2. Click and hold the left mouse button, and then drag the mouse pointer in the direction you want to move the camera. The display changes to an arrow, indicating the direction of the mouse.
  3. The further the mouse pointer is dragged to left or right, the faster the speed the PTZ will move.
  4. Release the mouse button when you have repositioned the camera to the desired location.