Light-Duty camera mount designed for wall mount applications

Issue

Does Pelco manufacture a light-duty camera mount designed for wall mount applications?

Product Line

Pelco Cameras

Environment

  • CM1450
  • Box Style Camera with 1/4-20 thread

Cause

Box camera is needed to wall mount and/or pole mount.

Resolution

Yes. The CM1450 wall Mount

Product Features

  • Low Cost Wall Mount
  • Decorator Styling
  • Supports up to 7 Pounds (3.2 kg)
  • Adjustable Swivel Head
  • Accommodates Light-Duty Cameras
  • Can be Adapted for Pole Mount Applications With Use of PA101 Adapter