What is the default baud rate for the CM9760-KBD Intelligent Keyboard?

Issue

What is the default baud rate for the CM9760-KBD Intelligent Keyboard?

Product Line

Pelco Matrix

Environment

CM9760-KBD Intelligent Keyboard

Cause

  • Configure the CM9760-KBD keyboard baud rate and parity for RS422 communication.
  • DIRECT MODE applications: The CM9760-KBD Default Parity of Even will cause No PTZ control of Spectra IV or new ES40/41 series cameras.

Resolution

The CM9760-KBD Intelligent Keyboards default RS422 communication settings are 4800 baud, EVEN parity.

View Lessons Learned Article LL#9747 for steps on how to change the CM9760-KBD Parity.