Is the IS110/IS111 Series camclosure an IP camera?

Issue

Is the IS110/IS111 Series camclosure an IP camera?

Product Line

Pelco Cameras

Environment

  • Camclosure 1 series

Cause

Video output options for IS110/111 camera.

Resolution

No. The IS110/IS111 Series are analog camera. Refer to the Cameras page for our network cameras.

The IP version of Camclosure 1 series was IP110-xxxx