When the DX8000 Client is opened it prompts with a The DX8000 Client is currently running?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

When the DX8000 Client is opened it prompts with a "The DX8000 Client is currently running"?

Product Line

Pelco Video Management

Environment

DX8000 Client

Cause

Execute file "DX8000C.exe" is still running on the PC.

Resolution

To fix the "The DX8000 client is currently running" prompts follow step below: 

  1. Press Ctrl+Alt+Del which will bring up the Windows Task Manager.
  2. Select Processes tab and look for DX8000C.EXE and End process.
  3. Close Task manager and re-open DX8000 client.