Can I install a Sarix IP camera into the EHX*E Series explosionproof camera enclosures?

Issue

Can I install a Sarix IP camera into the EHX*E Series explosionproof camera enclosures?

Product Line

Pelco Cameras

Environment

  • Sarix box cameras

Cause

Enclosure to support IP camera within explosion rated housing.

Resolution

Yes. Only the Sarix IX Series IP cameras can be install into the EHX*E Series. Refer to page 2, section Mechanical on the EHX*E Series Product Specification for maximum camera and lens size.