Problems can occur if LonMaker is not installed in the default directory

Issue

There have been some reports of problems encountered when LonMaker is installed in locations other then the default directory. These problems can include failure of LonMaker .dll files to register as well as plug-in registration failure.

Product Line

TAC Vista

Environment

Echelon LonMaker

Cause

LonMaker is not installed in default directory. Typically this refers to the C:\ drive, but it doesn't necessarily have to.

Resolution

Restrict the LonMaker installation to the default directory and the default LonWorks folder.

Example: C:\LonWorks