If I make changes to a video tie-line on a Multi Node system, do I need to reboot the CM9700-NW1?

Issue

If I make changes to a video tie-line on a Multi Node system, do I need to reboot the CM9700-NW1?

Product Line

Pelco Matrix

Environment

CM9740 Series Matrix system all versions

CM9760 Series Matrix system all versions

CM9765 Series Matrix system all versions

CM9770 Series Matrix system all versions

CM9780 Series Matrix system all versions

CM9760-NW1 all versions

CM9700-NW1 all versions

Cause

Changes to Node configurations or tie-lines have been made.

Resolution

Yes. The CM9700-NW1 will need to be rebooted so it can request an update from each node.