Are dip switch settings required for the CM9760-DT ASCII Data Translator to operate with the CM9700 Series Matrix Switcher?

Issue

Are dip switch settings required for the CM9760-DT to operate with the CM9700 Series Matrix Switcher?

Product Line

Pelco Matrix

Environment

CM9760-DT all versions

CM9760-DT4 all versions

Cause

What are the default settings for a CM9760-DT?

Resolution

No.

The CM9760-DT comes with factory default communication settings as follows:

– Odd Parity

– 9600 BAUD

– PIN 7777