What type of data input is required by the CM9760-CXTA Coaxitron Translator?

Issue

What type of data input is required by the CM9760-CXTA Coaxitron Translator?

Product Line

Pelco Matrix

Environment

CM9760-CXTA Coaxitron Translator

Cause

Installation configuration for the CM9760-CXTA

Resolution

The CM9760-CXTA Coaxitron® Translator will accept RS422 data in P protocol at 4800 baud rate or D protocol at 2400 baud rate.

PARITY settings:

  • EVEN for P protocol
  • NONE for D protocol