How do I enter Setup Mode on the CM9760-KBD Intelligent Keyboard?

Issue

Need to modify programming settings.

Product Line

Pelco Matrix

Environment

CM9760-KBD Intelligent Keyboard all versions

Cause

Setup issues

Resolution

To access the CM9760-KBD's Setup Mode:
1.  Turn DIP Switch 2 ON.

2.  Enter the setup PIN (default: 1234).

3. To exit select the door icon.