Starting a PTZ pattern using the CM9760-KBD Intelligent Keyboard.

Issue

How do I start a PTZ camera pattern using the CM9760-KBD Intelligent Keyboard?

Product Line

Pelco Matrix

Environment

  • CM9760-KBD Intelligent Keyboard
  • Pan, Tilt and Zoom Cameras

Cause

A pattern has been programmed in a Pan, Tilt and Zoom Camera and needs to be started.

Resolution

From the main menu on the CM9760-KBD LCD:
 
1.  Press the  button.
2.  If your camera support multiple patterns, enter the pattern number on the numeric keypad.

3.  Press the  button to start the pattern.