Access the programming menu on a CM6800 Series Matrix using a KBD960 Keyboard?

Issue

How do I access the programming menu on a CM6800 Series Matrix Switcher using a KBD960 Intelligent Keyboard?

Product Line

Pelco Matrix

Environment

CM6800 Series Matrix Switcher
KBD960 Keyboard

Cause

  • Forgot the default Logon password.
  • Requires matrix programming

Resolution

From a KBD960 Intelligent Keyboard:

  1. On the LCD, select MORE


     
  2. Select DEF


     
  3. Enter the Define PIN (default is: 1234)
     
  4. Select Menu.


     
  5. Select PGM, the blue logon screen appears.


     
  6. Enter the logon password, default is 2899100.


     

Note: Select PGM to exit out from the matrix menu