Issue
Can I use CM9765-VCC cards in a CM9760 bay?
Other questions may include:
- Since the CM9760-VCC is obsolete what is the replacement part number?
- I want to add additional camera inputs to my CM9760-MXB. What parts do I need?
Product Line
Pelco Matrix
Environment
- CM9765-VCC card
- CM9760-MXB bay
Cause
- Hardware Compatibility
- CM9760-VCC are obsolete
Resolution
No. The CM9765 components are not backwards compatible and cannot be used with a CM9760 Bay. Upgrade the matrix switch to CM9765-MXB and compatible components.