How to factory default the Net4001A.

Issue

How to factory default the Net4001A.

Product Line

Pelco Transmission & Power

Environment

NET4001A

Cause

Reset the encoder settings to factory default.

Resolution

To default the NET4001A you need to perform the following:

  1. Turn power off (by unplugging the cord)
  2. Turn the power back on
  3. Watch the Ethernet lights, when the red light goes out turn unit back off.
  4. Repeat this three times
  5. When powering the unit back up the fourth time, the IN red light will blink slowly.
  6. After this you can type the default IP address of the NET4001A into your browser (192.168.0.1)