Where are DIP switches located on a CM9760-ALM Alarm Interface Unit?

Issue

Need to set dip switches on a CM9760-ALM Alarm Interface Unit.

Product Line

Pelco Matrix

Environment

CM9760-ALM all versions

Cause

Addressing of the CM9760-ALM unit is required.

Resolution

The DIP switches are located behind the front panel of the CM9760-ALM Alarm Interface Unit.

They can be accessed by removing the five flat-head Phillips screws that hold the front panel in place.