Cannot call up monitor above 99 using CM9760-KBD keyboard

Issue

Cannot call up monitor above 99 using CM9760-KBD keyboard

Product Line

Pelco Matrix

Environment

CM9760-KBD (System 9700 Intelligent Keyboard)

Cause

The CM9760-KBD is in version 7 mode.

Resolution

Access the dipswitches on the keyboard and turn dipswitch 7 to ON position. By turning dipswitch 7 ON, it puts the keyboard in version 8 mode.