Locate the Digital Sentry software version running on a system

Issue

Where do I locate the Digital Sentry software version running on a system?

Product Line

Pelco Video Management

Environment

Digital Sentry

Cause

Confirm the current software version on the system before downloading the latest Digital Sentry software.

Resolution

  1. Navigate START > Programs > Pelco > DS Admin
  2. Log in with a valid Digital Sentry user account (default = Username: admin, Password: admin)
  3. Click on the Help menu and then select "About DSAdmin" in the sub menu.
  4. The About DSAdmin window will open and list the build version.

    The DigitalSentry version = 7.2.30 in this example.

     
  5. The DS Admin version is located at the top left corner in the title bar.