Check if Covert is enable on cameras using the DX4500/DX4600 Client

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Can I check from the DX4500/DX4600 Client to see if cameras on the DX4500/DX4600 Digital Video Recorder are configured covert mode?

Product Line

Pelco Video Management

Environment

DX4500/DX4600 DVRs

Cause

Useful troubleshooting step.

Resolution


Yes,

  1.  Login using an Administrator account.
  2. Once logged into the system, click on the Setup  icon.
     
  3. Navigate to the Camera  menu, determine if the Covert checkbox is checked or unchecked (enabled/disabled) .