What hard drive is installed in the CM9760/CM9700-CC1 Central Processing Unit?

Issue

What hard drive is installed in the CM9760/CM9700-CC1 Central Processing Unit?

Product Line

Pelco Matrix

Environment

CM9760-CC1 all versions

CM9700-CC1 all versions

Cause

Hard drive has failed.

Resolution

The CM9760-CC1 originally included a Western Digital 40GB IDE hard disk.  The current replacement part for the CM9760-CC1 hard drive is a Western Digital 160GB IDE hard disk.  The replacement drive can be ordered from Pelco using part number EE05-0201-2002G.