Restrict access to a monitor on the CM6700-MXB4 Matrix Switcher using the KBD300A keyboard?

Issue

Can access to a monitor be restricted?

Product Line

Pelco Matrix

Environment

CM6700 Matrix System all versions

KBD300A all versions

Cause

 Operators manipulating monitor views.

Resolution

The Matrix features a programming option of ACCESS. There are three programmable access functions.

  1.  KEYBOARD TO MONITOR  Access determines which keyboards have access to which monitors and if presets can be programmed.
  2. MON TO CAMERA 1-10      Access determines which camera images are shown on which monitors.
  3. MON TO CAMERA 11-16    Access determines which camera images are shown on which monitors.

NOTE: If not able to call up a camera on the CM6700 check the ACCESS on the monitor to camera or keyboard to monitor,Verfiy that access is set for Y.