Model number of a compatible fiber receiver to the FS85011AMST fiber transmitter.

Issue

What is a model number of a compatible fiber receiver to the FS85011AMST fiber transmitter?

Product Line

Pelco Cameras

Environment

  • FS85011A Series for Singlemode or Multimode Fiber Transmitter
  • Spectra III Analog Pendant Series
  • Spectra IV Analog Pendant Series
  • ExSite Explosionproof Analog Positioning System

Cause

Require a compatible fiber receiver for fiber connection to the FS85011A plug in module

   

Resolution

The FS85011A fiber transmitter features various models. Multimode and Singlemode. Review the following MODELS chart for compatible Receiver options:

  • View full FS85011A Specification Sheet here: FS85011A Sheet
  • View full FSF85011A Manual information here: FS85011A Manual
  • View full FR85011 Specification Sheet here: FR85011 Sheet 
  • View full FR85011 Manual information here:  FR85011 Manual
  • NOTE: FS85011AMSTEX, FS85011ASSTEX are recommended for factory installation.