How do I configure the initial setup on EnduraXpress EE500?

Issue

How do I configure the initial setup on EnduraXpress EE500?

Product Line

Pelco Video Management

Environment

  • EE500 Endura Express

Cause

Procedure on how to set-up the EE500 for the first time.

Resolution

Open a browser and connect to the EE500 web configuration interface. Default IP address is 192.168.5.10.
Log into web configuration interface.   The default password is admin
Once logged in to the EE500, you will enter the EE500 Setup Wizard.  Follow the steps in the wizard to continue setting up your EE500.

For more information, please refer to the EE500 Quick Start Guide.