What are the display options for the DVR5100 Hybrid Video Recorder?

Issue

What are the display options for the DVR5100 Hybrid Video Recorder?

Product Line

Pelco Video Management

Environment

DVR5100 Hybrid Video Recorder (HVR)

Cause

System's video output specification.

Resolution

The DVR5100 Hybrid Video Recorder supports two display outputs, Main and Sequence.

The Main display output supports VGA, PAL or NTSC video.  The Main monitor will connect to either the VGA, BNC or S-video port on the rear of the DVR5100.  This monitor can be used for all operator or administrator tasks on the DVR and is capable of multiplexed views up to 4x4.

The Sequence display output supports NTSC or PAL video.  The Sequence monitor connects to the Seq BNC output and cycles through cameras as defined in the DVR Settings, Seq.Monitor tab.