When using the CM9760-CXTA translator with the DX7116 DVR, do I have to match the video input on the DVR to the input on the CM9760-CXTA translator?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

When using the CM9760-CXTA translator with the DX7100 Series DVR, do I have to match the video input on the DVR to the input on the CM9760-CXTA translator?

Product Line

Pelco Video Management

Environment

  • CM9760-CXTA
  • DX7100 Series digital video recorder (DVR)

Cause

Video input of the DX7100 and CM9760-CXTA are used to create a line of communication between the camera and the DX7100.

Resolution

Yes, you will have to match the CM9760-CXTA translator video input to the video input on the DX7100 DVR to get the Coaxitron Signal to the correct pan and tilt camera.